I inherited a design in which a PTC is placed in series with the lowest battery in the stack. The bq20z90 system thinks it is monitoring that lower battery, but in fact, it is monitoring the cell voltage plus any drop across that 40mOhm PTC At Chg/Dsg current levels, it provides a noticeable offset, mid-tens of mV, and I see the CB bit flaring away, indicating a continuing, fruitless attempt at cell-balancing.
I think this is bad. Would anyone smarter than me happen to know what to expect with this dumb 40mOhm resistor sitting in series with my lower cell. i think this is going to skew the z-track, the cell-balancing algorithms and thus my capacity. What can I expect long term?
Golly, I wish they had put that PTC elswhere!
If I am fretting over nothing, I wish someone would tell me.
Regards,
Michael A. Banak