This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCR010505 does not start when using to isolate RS232

Other Parts Discussed in Thread: MAX232, DCR010505

I have used DCP010505 to isolate RS232 circuit, it means that isolated circuit was: MAX232 with capacitors and two ISO7221 and nothing more. It has worked well when RS232 cable from PC was connected to the circuit before power was on to the circuit.

I have thought that better choice is to use DCR010505 instead of DCP010505 and I did it. When I power on this circuit, and RS232 cable is connected to PC, it does not wake up (DCR010505 output voltage = 0V). When I disconnect RS232 cable from PC and connect it again to PC, DCR010505 wake up and work OK.

It is big problem because when there is short break down of the power, someone have to go and disconnect  and connect again RS232 cable it is not acceptable.

Perhaps I have to add something to the circuit or go back to DCP010505.

Please help me to solve this problem.

Stefan Pindera