We are seeing failures of this part where the PVIN shorts to gnd and the part smokes. The NC pin (5) in the design is floating. Could this cause failure?
-Jaden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are seeing failures of this part where the PVIN shorts to gnd and the part smokes. The NC pin (5) in the design is floating. Could this cause failure?
-Jaden
Datasheet is rather emphatic about the connect to GND:
5 NC These pins must be connected to GND to ensure proper operation.
Figure 35 in the datasheet shows the potential recirculating currents, so I would say it is quite possible NOT having pin 5 connected could result in failure, assuming all other design criteria is within the specifications.
-Leonard