Hello TI,
I'm developing a new product. I'm using TPA3111D1 audio amplifier and it needs 12V. So I have a Lipo single cell and I need Boost the voltage.
I've tested the TPS61085T but the problem is the Undervoltage lockout (2.6V).I've used 2 Sensing circuit :
-LMS33460MG . This one works but the problem is the noise at 3V.
-TPS3809K33. This one doesn't work.
But anyway the circuit of TPS61085T doesn't disconnect the load and the battery.
So I need a solution for the undervoltage lockout.
I have though in :
1.- LM5122
2.-Sensing circuit + solid state relay
What do you think? Whick one is better? Is there any solution for break the circuit at 3.0v?
Thank you very much