Hello,
I am curious about the pre-charge threshold of bq24630.
On the datasheet, it mentions when the voltage on the feedback pin is lower than VLOWV (0.35V typical), the charger will pre-charge. The problem is, for a 4 cell battery, the battery voltage(Vbat) needs to drop down to around 3.5V in order to achieve the condition ( Vfb < 0.35V). Normally, 9V is considered to be low on a 4-cell battery, is there any solutions on how to raise this threshold or LiFePo4 battery does not need this pre-charge function.
I have tried to change the resistor value at the output voltage divider, but it will also change the charging voltage. Also, I have tried to find other TI chargers for 4 cell LiFePo4 battery, but all of them are having the same threshold voltage (VLOWV = 0.35V typical) .
Thanks for your help!