Dear All,
I use UCC28019A to designed one 1KW PFC 。 I found that I can not add the load over 500W . if over 500W , the MOS will like a bump , not just burn . I enlarge the current shunt from 0.02 to 0.04 . AT first try to designed 2KW PFC , so the current shunt is 0.02 .what is the next step to Debug it . ( the curcuit is same as EVM . PFC inductor is 0.45MH.
PS . If I use the DC power supply , it work OK if dc Voltage is over 100, it will burn the MOS if I use the AC 110 power source .
Would someone explain it .