This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions about the bq51050bevm

Other Parts Discussed in Thread: BQ51050BEVM-764

Hi,

I'm using the bq51050bevm-764 module and I have some difficulties to understand where are the ports to connect an external load?

What does mean the AD external adapter exactly?

And what are the differences between rev B and rev C?

Thank you for your answers.

Best regards,

Guillaume.

  • Hi,

     

    OUT and GND (J4 and GND) can be used for the load.

     

    AD is used to send if there is any adapter connected at the input so that the wireless power will be disabled. Please find more details about AD and ADEN from the data sheet.

     

    The BOM is the only difference between the two versions and the B never been released

     

     

    Thanks

    Tahar