I am using the BQ2057 in the following circuit:
For some reason, when the power supply (VSUPPLY) is not attached, +VBAT gets connected to VSUPPLY.
I have figured a couple of things out.
- When Q4 is removed from the circuit, this problem does not occur. Of course, the batteries will not charge if Q4 is not in place so this does not solve the issue.
- There is no current flowing through R18 or D18. Therefore, current must be flowing into the SNS pin of the BQ2057.
- Removing R19 does not make any difference.
- Clearly the connection between VSUPPLY and +VBAT is being made through the BQ2057.
- Disconnection the VCC pin, the COMP pin, and the top of R19 from VSUPPLY and attaching them to the node between D18 and R18 did not solve the problem either. Replacing R19 with a 1k resistor also did not solve the problem. I have summarized some of my experimentation in the following tables.
VSUPPLY || VGS on Q4
--------------------------
0 || + 0.447 V
9.0 || - 0.796 V
VSUPPLY || R18 Current | R18 Voltage
0 || 0 mA | 0 V
9.0 || 0 mA | 0 V
VSUPPLY || R19 Current | R19 Voltage
-----------------------------------------
0 || 0 | 0
9.0 || 97.8 uA | 978 mV
Thanks in advance for the help!