Dear,
1. I try to use "UCC28600 QUASI-RESONANT FLYBACK CONTROLLER (Rev. J)", Excel Spreadsheet, for AC/DC Converter application. But I can't find out whom the recommended COMPONENT VALUES reference to. What EVM does this spreadsheet base on? Could you provide me that schematic?
2. What is the optimal de-rating percentage of switching MOSFET?
3. If I would like to design a transformer based on calculated with this spreadsheet, what considerations do I need to confirm? How do I chose core type and wire size?
Input: 85~265VAC
Output: 28V, 3A
Thanks and BR
David