This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210 for +/-150Vout, 500mAout

Guru 20090 points
Other Parts Discussed in Thread: TPS40210
Hello,
 
Can I use TPS40210 for below conditions?
I can't find any reference design and can't simulate by Webench.
-----
<condition 1>
Vin : 20V(min), 40V(max)
Vout : 150V
Iout : 500mA
 
<condition 2>
Vin : 20V(min), 40V(max)
Vout : -150V
Iout : 500mA
-----
 
If we can are there any refference circuit ?
If we can't are there any other device for above conditions ?
 
Best Regards,
Ryuji Asaka