Hi Folks,
TPS65023 datasheet indicates reset condition of DCDC1 is 1.225V if none of the workarounds are used (see page 43 of datasheet SLVS670J revised Sept. 2011) . I am not using any of these workarounds but measure 1.204V at VDCDC1 output on all 12 boards. VCC reaches 5V no more than 5ms prior to DCDC_EN being valid.
Do I still need to use one of these workarounds?
Any feedback on the conditions when these workarounds are not needed would be helpful, especially timing for Workaround #1.
Thanks,
Charlie