Hello,
I am using LM34922 switcher for two voltage rails. 5.4V@0.6A and 9.1V@0.4A. I designed the power supply using TI's webench tool and almost all the compoenets are same except some resistors due to availability. When I tested my first proto board, i was unable to get correct output on either supply voltage. I got 1.6V on 5.4 and 2.7V on 9.1. Currenty there is no load connected to it. Voltage at the FB pin is nearly 0.8V for both the supplies. Input voltage is 12V.
I tried with external load and varied it between 0.2A to 0.6A on 5.4V regulator. In this case output voltage tried to increase but it could reach up to 4.6V only and not to 5.4V. Also LM34922 chip was heating too much when I connected axternal load and also making some humming noise which inceased as the load increased.