Hello,
I know I need to use one TPS7A4700 per converter but in regards to the FPGA I have a few questions.
1) I need to cover 12v, 2.5v and 3.3v. Could the TPS7A4700 be set to 1.2v using a ext resistor or would you recommend a different part. Clean low noise is important.
2) Can the TPS7A4700 be cascaded to cover a larger power draw?
3) Would a supercap on either or both input and output help during times of high pwr draw in addition to the recommended configuration?
The total draw is estimated at 3 watts on the FPGA for all 3 voltages. I might get by with one TPS7A4700 per voltage but not sure at this point which is why I asked questions 2 and 3.
Thank you,
Tom Hurst