Other Parts Discussed in Thread: EV2400, BQ27531EVM, BQEVSW
I have seen quite a few posts here on the forums regarding compatibility issues between the EV2300 and different OS versions (Windows XP, 7, 8, 32 bit, 64 bit, etc). It seems as though the EV2400 is newer and thus works "out-of-the-box" with more operating systems.
I would like some clarification about the following:
1) What OS versions is the EV2300 *actually* compatible with as of this time? My main OS is 64 bit Windows 7 and it would be nice if the EV was compatible with that OS. However, I have an older computer using Windows XP that I could set up for use with the EV2300 if that is the only compatible OS version (although I'd much prefer to not need to do this).
2) What are the differences between the EV2300 and EV2400? I am planning on using it with the BQ27531EVM, which seems to be compatible with both EVs. Do I need the EV2400 or would the EV2300 suffice?
3) The EV2400 was $49 as listed on its product detail page a few weeks ago. Now, however, the price has jumped to $200. The various distributors (Digikey, Mouser, etc) also showed this phenomenon of 400% price increase recently. What difference from the EV2300 makes it twice as expensive? Why the huge price jump?
Thanks.