Hello,
I want to use LM2623 to step up 5V to 5.9V. Current drive required is 2A.
Will this regulator support 2A at 5.9V. Because in data sheet its mentioned as
Please reply at the earliest.
Thanks & Regards,
Ajith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I want to use LM2623 to step up 5V to 5.9V. Current drive required is 2A.
Will this regulator support 2A at 5.9V. Because in data sheet its mentioned as
Please reply at the earliest.
Thanks & Regards,
Ajith
Hi Ajith,
I'm not the design center support, but came across this with no response so step in to help out. There is no particular info on DS, but from your input of 5V and Vo of 5.0V which is not very high, so can be decuced as YES.
It should deliver 2A, try use the LM2623A version which has higher current limit of 2.2A instead of 1.2A typ would make it a better choice. Hope that answer your query.
Kern