I implemented a basic adj circuit, r1=120ohm(output to gnd pin), r2 = 5k pot (ground pin to GND).
It was working on first tests, on a 12V source I could move it anywhere from 1.25V to ~11.5V with the pot.
Now its stuck at max, always Vin - 0.3V. I see no burning or overheating, the regulator gets I'd call very warm after about 2 min with no direct load.
Is it the regulator or something else? (I've confirmed that the pot works fine)
Thanks.