This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53319 Power On with 12V

Other Parts Discussed in Thread: TPS53319, TINA-TI

Hello, i am interested in using the TPS53319 for my application. I want to power it with a 12V source and step down to 5V10A. The problem is, i can use a maximum of 6.5V for the EN Pin (datasheet), so i can not connect my 12V directly to the EN Pin. Now i wonder if it is possible to connect the VREG Pin to the EN pin, because VREG Voltage seems so be independend of EN to get the device working...

Greetings