Need some tech assistance on the pretty simple part TPS60403.
Using it for at most 30ma supply, to be the negative rail for three op amps and the 250khtz is leaking into the laser diode optical output.
Have 4.5v going in, get negative 3.8v out loaded, which is fine.
If I leave the circuit on the board and just pull the output pin, and use an external negative linear supply, laser is clean.
Have the exact LC post filter shown in fig 25. Have since tried varying Lp and Cp without much change.
Also the filtered output goes to a Murata 3 terminal 1uf cap for additional filtering.
Haven’t seen the noise on the op amp output but added some filtering there just in case…..nothing.
Data sheet didn’t say anything about ground plane, the component does share that.
Any suggestions ?