Other Parts Discussed in Thread: UCD3138, UCC28950, UCD3138064, UCD3138PSFBEVM-027
I'm currently designing a full bridge phase shift converter, so far I have tested UCC28950 but I think it will be worthwhile to use the UCD3138 family instead,
especially since I will need to control the converter with a serial interface anyway.
I have now the UCD313806EVM-board which I will connect to the converter.
My questions:
- I would like to have some sample source code to start with. Do you have anything to share, preferably a working project for the latest CCS version...
- When using digital fusion, I can find the device on the EVM board only when I scan in ROM mode (using the UCD3XXX/UCD9XXX Device GUI) but not otherwise. So I can't start digital fusion in on-line mode. Any idea?