Hello all,
I used Webench to make the circuit of a DC/DC with:
- 14-14V Input.
- 7.6V Output.
- 20A Output.
But... it doesn't work, seems to have all pins with 0V but EN is about 1.5V. I made 2 different PCBs but not working.
The schematic is this one:
Can be a problem with Diode? Attached is the file I got from Webench.
6471.WebenchReportsServlet.pdf
In the output I only have about 0.3V
Best Regards!