the 3.7V battery is running at full load with 2A current/ 3.4V, while the 5V adapter plug in, the system output have undershoot, the voltage down to 2.8V, then go up to 5V. from AC to battery, the system output doesn't have any undershoot issue. However, after some adjustment for gate to source of the ACFET , the battery to AC undershoot problem is almost solved, but, AC to battery have some undershoot under 3V. since our system DC/DC works above 3V, this undershoot cause system unstable.
Is there any way to solve the system power auto selection undershoot issue?
thanks ,
Jun