This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24140 USB OTG boost powered by Vin?

Hello All,

Pretty much as the title says... The datasheet describes how the battery can power a USB OTG port (boost mode), which is part of what I need. I also need the part where the battery and/or system is powered through Vin. So, can these be combined? What if Vin is present, I want the battery to be charged and I also want the USB OTG boost to be active... I suppose the hardware is there (FETs etc), but does it work? And is this supported in the registers/SW?

YAY/NAY?