Other Parts Discussed in Thread: BQ24010
I am using the following scheme.

the battery pack has protection from overcharge and overdischarge.
in the case of discharge , protection disconnects the battery. If Input voltage(5V) connect Vout from BK24010 is 1.3V That is not enough for what discharge protection connect the battery.
in the case of a battery disconnected from the board at Vbat = 1.3V
If I disconnect the R17 - the charging Voltage is normal.
U3 consumption not more than 100 mA. how can I fix this problem?