Hi guys,
This probably very noobish question but I have been wondering this many times and actually run to it now when I wanted to use LM2832XMY in my design. I'm using 8-Pin eMSOP-PowerPAD where there are 3 GND pins.
The question is should I use just one GND pin in my layout or are all the 3 pins needed? I'm guessing that only one is needed depending which one of them fits the best in the layout. I just haven't ever seen a text where it says "use only one which fits your design" or maybe there is but i haven't found it. Maybe you can guide me to the answer :), thanks.
Br,
Matti