What's the difference between TPS56121 and TPS56221, apart from the different possible output current? I use this components with output currents up to 12Amps, well below the max. output current of 15A (TPS56121) or 25A (TPS56221). We want to validate the design with one type, but want to use the other as well, if there is no stock at TI/ distributor. Would be nice if they are interchangeable.