Hello!
I tried to configure the TPS54360 for 3.3V / 3A. With no load the output voltage seems fine but when the output curretn rises Vout falls to something about 2.6V. For the design I used the eq in the datasheet.
f=580kHz
L=10uH
RHS = 167.5kOhm
RLS = 53.6kOhm
Cout = 100uF
I use the EVM for testing. I tried also a higher inductor but with no effect.
Is there something else to take into account when desgining the curicit?
Kind regards
Paul