Hi, I'm trying to simulate a dual output power supply (12V and 5V each at 2A) using the TPS54383 (schematic on page 42 of the datasheet. Datasheet can be found here - http://www.ti.com/lit/ds/slus774b/slus774b.pdf). A bridge rectifier supplies 24Vrms to the PVDD1 and 2 pins. This is a sine wave source simulating the secondary of a step-down transformer. However the output waveforms are very choppy and they seem to be switching with the rectifier (please see the attachment). When I remove the bridge rectifier and make VG1 a unit step source of 24V DC, everything works great. What is going wrong here?