This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"VDDCtrl voltage selection register" setting value of TPS659113

Hi~

Our customer use TPS659113.

If you see attached file on page77(Table 50. VDDCTRL_OP_REG, Table 51. VDDCRTL_SR_REG), it mentioned as below.

Vout= (SEL[6:0] × 12.5 mV + 0.5625 V)

If SEL[6:0] = 0110001, Output voltage is mentioned as 1.2V

But, According to formular, Actual output voltage is 49*12.5mV+0.5625V = 1.175V

I think that SEL[6:0] value for 1.2V Output voltage is 0110011.

Please check this question.