Hi, I need the thermal resistance from junction to case (theta-jc) for LP3882MRX-1.2/NOPB. The datasheet provide only junction to ambient.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I need the thermal resistance from junction to case (theta-jc) for LP3882MRX-1.2/NOPB. The datasheet provide only junction to ambient.
The requested junction-to-case thermal resistance (theta-jc) for LP3882EMR-x.x (SO PowerPAD) is not immediately available. I have submitted a request for thermal simulation today, but that can take up to two weeks to complete.
There is no "LP3882MR..." that I can find. I believe that you may have meant "LP3882EMR...":
LP3882EMR-x.x SO PowerPad
Theta JC, top = 49.5°C/W
Theta JC, bottom = 2.1°C/W