This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AC-DC Convertor with high efficieny using UCC28600



Presently we are doing a SMPS project for well know institution along with state government for a rural power product for India. They are projecting a initial volume of 10K at start up for trial run. Once the design is proven there will be a huge volume.
In that regard we have already submitted our present 150W (48V @ 3Amp) CV SMPS for their
demo purpose which is working fine but bulky in design.
Looking at the end product spec. we need the meet
1) High efficiency
2) Small foot print
3) Low thermal
4) Best price.
5) Easy manufacturing
Thanks and Regards