Hello
I am making a board using the bq27541DRZT-V200. We have now built around 1K and are going to run another 3K next week. Referring to the reference schematic on page 36 of the data sheet. What would be considered the acceptable capacitance range for C1,C2,C4,C5 and C7? This application is a very tight fit. I am having a hard time finding 0.1mfd thin enough to clear. Oddly, I have found 1000pf and 0.47 mfd in thin enough packages. Also, when I made the board, I did not put a place for C11 and C12. What are the possible consequences?
thanks
dpk