I would like to use DC source to replace AC source to test PFC converter using UCC28070. In this case, I can fixed Vin to a DC level such as 100V. The output should be a regulated 400V no matter Vin is 100V or 200V because PFC is a boost converter.
I am not sure Vout is still regulated when the input is a fixed DC, considering a multiplier is involved in the loop.
My question is:
May I use DC source instead AC source to test a PFC?
Thank you in advance for your answer.
Sam Guo