Dear all!
I made a power supply use two 2576 ADJ for my fuzzs. I use a transformer 220V to 18V/ 5A (AC), output voltage of diode bridge is 20-22V DC, capacitor after diode bridge is 2200uF. Output voltage of the power supply is 9V and I made 4 outputs from each 2576.
If I use all 4 outputs of a 2576, it's OK. But when I use 2 outputs of a 2576 and 2 outputs from another, it's so noise in my amp. I think having some problem in output power, my fuzz is Boss GT2, Boss NS2, Boss DD 20 and TS7 Tubescreamer
Can you help me fix it?
Thank you!