This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reverse polarity protection for TPS62133

Other Parts Discussed in Thread: TPS62133

The absolute minimum voltage rating for the AVIN and PVIN pins on the TPS62133 is -0.3V.

Does this mean that a voltage of -9V applied to the AVIN and PVIN pins will damage the device?

If yes then I will have to add a reverse polarity protection circuit.