I'm using bq27531 with bq24193 in a standalone configuration. I use a circuit similar to the one in the bq27531 spec sheet. I ran into a problem where an overcurrent situation caused the system to shut itself down (As it should). My problem is that the only way I had to reset the system was to switch off the battery/charger. Any reset button in series with those components would need a high current rating, and that makes for an expensive switch. Is there a good way to reset the system without I2C communication or reset button in series with the adapter/battery?