This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27530 autocycle option in bqevsw

Other Parts Discussed in Thread: BQEVSW

Hi

I want to teach my bq27530evl my battery.

I wanted to do a learning cycle but coudnt do it manually using 0021 command.

I am wondering does the autocycle in the bqevsw refeering to learning cycle?

is not what does it mean if yes, it is written there :


**************************************************
Autocycle without Relaxation times - 1 output pin
**************************************************

Hardware Setup:
The EV2300 I2C-VOUT (E2-VCC) terminal should be connected to a transistor/FET switch
or relay which will connect your load to the battery pack when the signal is HIGH (+5V).
Your charger should be connected to the battery pack when the signal is LOW (0V).

what does it mean?

do I need to disconnect jp1 jumper? and connect the transistor gate to the I2C-VOUT pin?

it doesnt make any sense to me because this pin in connected to ground in the evl so what does this mean????

Thanks in advanced