Hi,
I need help choosing a controller for the synchronous buck power supply.
As you can see in the title so it must have wide input voltage range, 33-100VDC.
Out will be 24V and 10 to 15 A load.
There shall be two phase that runs at 180 degrees. Currents sharing is important.
I looked at the TPS40140 which might make it but not shure.
Grateful for any suggestions.