Hi,
We have an OTG USB design, and would like the board to be able to act as USB HOST even when powered only by 3.7V lithium battery.
This means we need an IC to buck-up from 3.7V to 5V for USB VBUS power supply to the USB peripheral. The peripheral is only going to be a USB flash drive and presumably would require much less power than 500mA. Could someone recommend a power IC (the simpler the better) for this purpose?
Additionally, probably we also need a current-limited (to prevent current from exceeding 500mA) switch for this purpose. Does any buck-up power IS also have current limting ability built-in for this purpose?
Paul