I'm having an issue where the bq77908A is drawing current on the VC8 pin. It is in a 8 cell configuration. We connect the circuit by connecting VSS and BAT/PACK+ first and then the cells from bottom to top.
Once attached, we see the VC8 pin drawing current and it usually comes out on VC9 (measured on the sense resistor), other times it is a significant current to see on the VC8 series resistor but nothing appears on VC9 and all other signals are fine.
Is there anything that may cause the bq77908A to behave this way? I have disabled the flag for cell balancing on this still occurs. This also occurs both on simulation resistors(where the current draw causes under/over voltage faults) and live cells.