Hi,
I am trying to test UCC2891 PWM output before using the chip to build the dc-dc converter. In my bare bones circuit i have placed the following components Rdel, Ron, Roff, Rin1, Rin2. All other pins are made floating.
I also connected a 10uF capacitor at the VDD pin. When i turn ON the supply 24V @Vin pin the voltage at VDD pin goes upto 5V and stays at this point.
As per the datasheet the VDD pin voltage needs to go upto 13.5V for the device to turn ON.
Can somebody figure out the reason why this is the case ?
Also, the device consumes excessive current if i try to connect VDD pin directly to the supply of 24V.
Thanks,
Kurian Polachan