Other Parts Discussed in Thread: LM2623
How can I transform an LM2623 into a buck-boost topology by using this example diagram?
An LM2623 has the EN pin connected to the output and has a single GND.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LM2623 should work in this application; although I do not know of anyone who has tested it.
Be careful about the maximum input voltage on the gate of Q1. The abs max on the LM2623 EN pin is 10V; so
it can be connected to Vin if that restriction is respected.
FD
Problem is, the input voltage is variable (cells) I noticed that the output drops a few 100mV when voltage on EN pin drops.
How can I limit the voltage on the EN, BOOT and Vdd and FB pins without limiting the output voltage?