Hi all,
I am having some problems getting my LM3409 design to work properly.
Spec is:
12V in (11V to 14.5V specified)
8V-10V out (issue with 11V in, I know)
120mA - 2.3A range for the current, adjusted via IADJ pin, to adapt different LED rails
PWM 100 Hz - 1kHz for brightness control
My problem is that current regulation is not stable over the input voltage range of 11V - 14.5V. The output current is ok at 12V nominal voltage, but varies in a non-linear way with input voltage.
I am right now testing with a 2.8 Ohms resistive load and 1.2A current (V_IADJ 620mV).
When increasing Vin to reach the limit of 14.5V, at some point the current increases very fast and then further runs off the scale (due to some thermal effects?), only to be stopped by me at around 2.5 A by turning down the input voltage.
Strangely, this does not happen when setting the current to 2.3A, at this operating point I can increase the input voltage up to 16V with the current increasing somewhat linear with the voltage, but not seeing a trip point like in the above case.
Did anybody else experience such behaviour? What might be the cause, in which direction should I investigate?
V_IADJ is constant, measured directly at the IC pins.
Any help is appreciated, I am out of ideas!
Best regards,
Wolfgang