This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

question about mppt using of sm722445 and bq24650

Other Parts Discussed in Thread: SM72445, BQ24650

hi,

 I test  the sm72445  evaluaion board ,when input is above 30V and without load connect output ,the input  consume current is above 100mA, I think may be some trouble ,how do you think? 

The other question is about BQ24650,when i use MOSFET IRL7833 replace the SI7288,  the input  consume current is more than 20mA,that is why ?IRL7833----Qg=32nc,RDS(on)=3.8mΩ,Ciss=4170pf,Coss=950pf,Crss=470pf.