I have a BQ24105 soldered into a PCB I designed according to the attached schematic. For the most part the charger seems to work fine when using a 12V battery as a supply (other than some charge termination concerns [see my other post for more details on that http://e2e.ti.com/support/power_management/battery_management/f/179/p/274388/1028282.aspx#1028282]).
However, when I connect a solar panel (~10V during testing) to the supply input, Stat1 and Stat2 are both high indicating a fault. If I put a multimeter on the nPG pin I see that the voltage is generally low, but it jumps around and seems to go high for short periods of time.
Measuring the current shows that only about 8mA of current is being drawn from the panel, so it is clear the charger is in a fault state and not charging.
What would cause this behavior? The solar panel has a Iid of 290mA and a Isc of 360mA. Having measured the current from the battery I do notice that there is about 500mA being drawn during charging. Is the fact that the solar panel is not able to produce this much current causing the chip to shutdown? I assumed I would just receive a slower charge if the input current was limited.
Is there any way around this, because I need to be able to charge from a solar panel?