Hello,
Can you provide the θjc value of TPS3808G01DBVR?thanks!
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joyce,
Please note that as TPS3808 is a supervisor, there will not be much dissipation through the device. Here are the thermals for the DBV package:
Theta JA | 180.9 °C/W |
Theta JC | 117.8 °C/W |
Theta JB | 27.8 °C/W |
Psi JT | 18.9 °C/W |
Psi JB | 27.3 °C/W |
Very Respectfully,
Ryan