Good day,
I was curious if anyone has any suggestions about implementing PFC on a TPS54260 design (output is 20V @ 1.2A)? The design is relatively straightforward where the TPS54260 is fed from a full wave rectified 24VAC signal. I just started prototyping the design and my initial tests show a PF of 0.74 which is OK, but I would like to improve this if I could. Any suggestions, as I have not done PFC before and so I am a noob...
Thanks in advance!
Cheers,
Sam