This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reducing output ripple on the TPS54383

Expert 1350 points
Other Parts Discussed in Thread: TPS54383

I simulated the TPS54383 using the schematic on page 33 of its datasheet. However there is a significant ripple in the output voltage - 500mV for the 3.3 output and 800mV for the 5V output. I know that there is a restriction on the max output capacitance but any way I can reduce this ripple? This ripple is non-existent when I simulated a variant of this circuit that has 12V and 5V outputs. I've attached the 5V and 3.3V output circuit and the waveforms here.

TPS54383.zip