Hello,
based on LM2576 with which constant current can be easily achieved, I have got a question:
I would like to make almost similar construction but with current of at least 8A.
Typical Input would be 12-14V up to 28V.
Coverter will drive LED - each 10V, 1A connected paralelly.
Which SIMPLE SWITCHER would fit this goal and if non any other that would be affordable?
Maybe cheaper would be tide together 2 or 3 cheap SIMPLE SWITCHERs (like LM2576) but how to do it.
Thanks and waiting for reply!