This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61222 stability of the output?

Other Parts Discussed in Thread: TPS61222, TPS61260, TPS61070

Dear ,

I am afraid , thanks in advance , please comment on this

In TPS61222 step-up converters to power LEDs from a AAA 1.5V battery (step-up to 5V).

We would like to know more about the stability of the output voltage V_out when it is set to 5V.

I seen the  range of 4.82 to 5.13V in datasheet, but that seems to be a population-level statistic (including variation between units).

Would anybody  able to provide an output voltage range / variation for a) A single TPS61222 unit through its entire life b) A single TPS61222 unit over a short period of ~5