This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Li-ion battery charger selection.

Other Parts Discussed in Thread: BQ24600, BQ24610

Hi TI team,
I need some help in selecting Li-ion battery charger . I am designing an analog board which requires +5V and -5V. The board shall be powered ON from 230V AC and there should be provision for powering ON the board from ON board battery also.
I am using an AC adaptor which gives +12V DC. I am using 2 lithium-ion batteries(4.2V) in series which gives 8.4V and then will use buck converter for deriving +5V. Now, my requirement is to select a battery charger for charging 2 litium-ion batteries. So, please suggest me a battery charger which meets this requirement. OR is it good practice to use single battery and single battery charger and then use a boost converter for deriving +5V from battery's 3.7V or suggest any alternative. Maximum current derived for +5V would be 1A.

Thanks,

Shashank